Technical FAQs

Ask a Question

What type of hub is used with the NEMA 3R, rainproof HOMELINE load centers?

Issue:
Accessories

Product Line:
Homeline load centers

Environment:
Hub Types

Cause:
Installation

Resolution:
The NEMA 3R, Rainproof HOMELINE load centers have a suffix RB in their catalog number. The 'R' designates a Rainproof enclosure and the 'B' designates the load center uses a bolt-on, type B-Hub. The B-Hubs come is sizes from 3/4" up to 2-1/2". The Catalog numbers of the B-Hubs is based on the size, see below for the sizes and catalog numbers. A closing Cap(catalog number BCAP) is provided with ALL 'RB' suffix catalog numbers.

B-Hub Catalog numbers:
The 3/4" is B075, the 1.0" is B100, the 1.25" is B125, the 1.50" is B150, the 2.0" is B200 and the 2.50" is B250.


CTA-ID : 11856
Was this helpful?
What can we do to improve the information ?