Technical FAQs

Ask a Question

Is 230 volt replacement control coil available for LC1D15000?

Yes, order LX1D8P5 for 50 hertz or LX1D8P7 for 50/60 hertz. Average coil consumption is 300 VA inrush 22 VA sealed for 50 hertz, 300 VA inrush 22 VA sealed for 60 hertz and 280 to 350 VA inrush 2 to 18 VA sealed for 50/60 hertz.


CTA-ID : 11303
Was this helpful?
What can we do to improve the information ?