Technical FAQs

Ask a Question

Is 440 volt replacement control coil available for LC1D25008?

Yes, order LX1D4R5 for 50 hertz, LX1D4R6 for 60 hertz or LX1D4R7 for 50/60 hertz. Average coil consumption is 90 VA inrush 7.5 VA sealed for 50 hertz, 1000 VA inrush 8.5 VA sealed for 60 hertz and 100 VA inrush 8.5 VA sealed for 50/60 hertz.


CTA-ID : 11700
Was this helpful?
What can we do to improve the information ?