Technical FAQs

Ask a Question

Is 32 volt replacement control coil available for LC1D25004?

Yes, order LX1D4C5 for 50 hertz. Average coil consumption is 90 VA inrush 7.5 VA sealed for 50 hertz, 1000 VA inrush 8.5 VA sealed for 60 hertz and 100 VA inrush 8.5 VA sealed for 50/60 hertz.


CTA-ID : 11532
Was this helpful?
What can we do to improve the information ?