Technical FAQs

Ask a Question

Is 480 volt replacement control coil available for LC1D25004?

Yes, order LX1D4T6 for 60 hertz. Average coil consumption is 90 VA inrush 7.5 VA sealed for 50 hertz, 1000 VA inrush 8.5 VA sealed for 60 hertz and 100 VA inrush 8.5 VA sealed for 50/60 hertz.


CTA-ID : 11709
Was this helpful?
What can we do to improve the information ?