Technical FAQs

Ask a Question

Is 400 volt replacement control coil available for LC1D6511?

Yes, order LX1D6V5 for 50 hertz or LX1D6V7 for 50/60 hertz. Average coil consumption is 200 VA inrush 20 VA sealed for 50 hertz, 220 VA inrush 22 VA sealed for 60 hertz and 245 VA inrush 26 VA sealed for 50/60 hertz.


CTA-ID : 11383
Was this helpful?
What can we do to improve the information ?