Technical FAQs

Ask a Question

What are the repair parts for a H367NAWK Series E4 Heavy Duty Safety Switch?

Issue:
Repair parts

Product Line:
HD Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 44011-197-50 (3-required and arc suppressor assembly is not included)
Load base assembly - 44011-393-50 (3-required)
Arc suppressor assembly - 44011-394-50 (3-required)
Lug assembly - 44050-053-02 (1 required per base assembly)
Neutral assembly - H800SNE4
Line base phase barrier - 44011-195-01 (2 required)
Line base insulating plug - 44011-339-01
Handle assembly - 44011-391-50 (Obsolete - replaced by 44011-413-51)
Door thumb retainer - 44050-490-01
Door thumb screw - 44050-434-01
Handle knob kit - 40283-435-50 (the black & red knob at the end of the handle)
Neutral bonding strap - 44011-342-50 SEL
Crossbar Insulator Kit - 4051275250 (note: the metal cross bar is not replaceable)
Fuse Mounting Hardware - Bolt = 2140128481, Nut = 2342702800, Washer = 2360100280


CTA-ID : 12590
Was this helpful?
What can we do to improve the information ?