Technical FAQs

Ask a Question

Can the cover of a LA400AWK circuit breaker enclosure be padlocked closed?

Issue:  
Can I access the interior of the LA400AWK enclosure while the breaker is closed (in the ON position)?

Product line:  
Circuit breaker enclosures

Environment:  
L-frame breaker NEMA 12/3R enclosure

Resolution:  
Yes, the cover is provided with an integral padlock hasp for locking the cover closed.  There is an interlocking feature which prevents the cover from being opened while the breaker is closed (in the ON position).  
Was this helpful?
What can we do to improve the information ?