Technical FAQs

Ask a Question

What is the part number for the NEMA Type 1 QO and HOMELINE load center cover mounting screw?

Issue:
Repair Parts

Product Line:
QO and HOMELINE LC

Cause:
Maintenance

Resolution:
The 3/4" long screw used with flush and combination covers is 4020513002K. The 1/2" long screw used with surface covers is 4020513001K. These cover screws are a special triple lead, thread-forming screw that is only available through authorized Square D distributors. A quantity of 10 screws is provided when ordering either 4020513001K or 4020513002K.




CTA-ID : 13191
Was this helpful?
What can we do to improve the information ?