Technical FAQs

Ask a Question

Are NEMA 1 enclosed 8910DPA contactors available from the factory?

Yes, up through the 90 amp version. Add a ``G`` to the part number, i.e. 8910DPA12V02 becomes 8910DPAG12V02.


CTA-ID : 14412
Was this helpful?
What can we do to improve the information ?