Technical FAQs

Ask a Question

Are closing plates available for the rectangular 9999S cover mounted control units?

Product Line:
 
NEMA style starter cover mounted control units
 
Resolution:
 
Select appropriate closing pate from detail listed below:

9999SG3 - This closing plate kit is designed to re-close the indicated knockout on the following enclosures:

Class 8538/8539 Size 0 thru 4 NEMA 1 combination enclosures
Hole Function: 2 or 3 Position Selector Switch & Start/Stop Push Buttons

Class 8903 NEMA 1 - 30A thru 200A Type S combination enclosures
Hole Function: 2 or 3 Position Selector Switch & Start/Stop Push Buttons

Class 8941 Size 0 thru 4 NEMA 1 combination enclosures
Hole Function: 2 or 3 Position Selector Switch & Start/Stop Push Buttons

9999SG2 - This closing plate kit is designed to re-close the indicated knockout on the following enclosures:

Class 8502/8536 Size 00 thru 3 NEMA 1 enclosures with slip-on cover designs
Hole Function: Pilot Light & Reset Lever

Class 8502/8536 Size 0 thru 1 NEMA 1 oversized enclosure (Class 9991 SCG1)
Hole Function: Pilot Light & Reset Lever

Class 8538/8539 Size 0 thru 4 standard NEMA 1 enclosures
Hole Function: Pilot Light

Class 8903 NEMA 1 combination enclosures (30A thru 200A)
Hole Function: Pilot Light

Class 8903 NEMA 1 non-combination enclosures (30A thru 100A Type S)
Hole Function: Pilot Light

Class 8941 Size 0 thru 4 NEMA 1 combination enclosures
Hole Function: Pilot Light

9991SG3 - This closing plate kit is designed to re-close the indicated knockout on the following enclosures:

Class 8502/8536 Size 00 thru 3 NEMA 1 enclosures with slip-on cover designs
Hole Function: 2 or 3 Position Selector Switch & Start/Stop Push Buttons

Class 8502/8536 Size 0 thru 1 NEMA 1 oversized enclosure (Class 9991 SCG1)
Hole Function: 2 or 3 Position Selector Switch & Start/Stop Push Buttons

Class 8903 Type L\LX NEMA 1 enclosures with slip-on cover designs
Hole Function: 2 or 3 Position Selector Switch & Start/Stop Push Buttons

Class 8903 NEMA 1 non-combo enclosures
(30A - 100A Type S Electrically Held Only)
Hole Function: 2 or 3 Position Selector Switch & Start/Stop Push Buttons



CTA-ID : 14217
Was this helpful?
What can we do to improve the information ?