Technical FAQs

Ask a Question

What is the suffix for faston connectors for the D-line contactors?

Suffix ``9`` should be placed at the end of catalog number (i.e. LC1D09109G7, LC1D099G7, LP1D09109BD, LC1D099BD) before voltage code. Faston connectors are only available on 9 & 12 amp (D09 & D12) AC3 rated contactors. Additionally, the addition of faston terminals voids UL Listing but provides device with UL Recognized designation.


CTA-ID : 14260
Was this helpful?
What can we do to improve the information ?