Technical FAQs

Ask a Question

How does the GV7V01 locking device mount?

The attachment is installed above the toggle when in off position. There are slots in the toggle recess. When the attachment is inserted and closed there are legs, which spread out into slots of the recess and prevent the toggle from being opened. Up to 3 padlocks with shank diameter of 5 to 8 mm (0.2 to 0.3 in.) can be used.


CTA-ID : 14273
Was this helpful?
What can we do to improve the information ?