Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 82354 Double Throw Safety Switch?

Issue:
Product Design features

Product Line:
Double Throw Safety Switches

Environment:
Lug wire size

Cause:
Installation

Resolution:
The lugs on this device will accept (1) #6 AWG - 300 kcmil Aluminum or Copper conductors per phase. There are NO alternate lugs


 
Was this helpful?
What can we do to improve the information ?