Technical FAQs

Ask a Question

Is the FP221R suitable for use as service equipment?

The device is suitable for use as service equipment on a 120/240Vac, 1ph-3w service if used only on a 1ph-2w load; and only when the equipment grounding terminal supplied is replaced with ground bar kit, catalog number PK3GTA1.


CTA-ID : 15085
Was this helpful?
What can we do to improve the information ?