Technical FAQs

Ask a Question

What are the repair parts for a 82344DS, Series E1 Double Throw Safety Switch?<br />

Issue:
Repair parts

Product Line:
Double throw switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Blade assembly - 40538-165-50
Top switch base assembly - 40538-132-51
Bottom switch base assembly - 40538-133-51
Arc suppressor assembly - 40538-189-50
Handle knob assembly - 40284-357-50
Lug assembly - 40251-162-51
base mounting screws - 40205-065-01


CTA-ID : 15390
Was this helpful?
What can we do to improve the information ?