Technical FAQs

Ask a Question

Q13100VH Circuit Breaker Replacement

Issue:
What is the replacement circuit breaker for the Q13100VH in an obsolete NQO panelboard?

Product Line:
Obsolete NQO panelboards that were sold and supported in the USA.

Environment:
Replacement/maintenance.

Cause;
Are specific branch circuit breakers still available for the obsolete NQO panelboards?

Resolution:
If used as a branch breaker in an NQO panelboard, use a QO3100VH with the SK5669 mounting kit.  


CTA-ID : 15741
Was this helpful?
What can we do to improve the information ?