Technical FAQs

Ask a Question

What are the repair parts for the HU364DF, series E1 (may be shown as E01)?

Product Line:
Heavy Duty Safety Switch catalog number HU364DF, Series E1

Cause:
The repair parts numbers for the HU364DF, series E1, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable.

Resolution:
The repair parts for the HU364DF, series E1 (E01) are as follows. These are the parts that can be replaced. No other parts are replaceable.
-Interior Assembly - 9422TF1(includes the line base, mechanism and operating rod)
Was this helpful?
What can we do to improve the information ?