Technical FAQs

Ask a Question

Are NY1B panelboard replacement breakers still available?

Issue:
Replacement breakers

Product Line:
Panelboards

Environment:
NY1B

Cause:
Obsolete panel

Resolution:

The 1-pole 15-50A Y1B breakers are obsolete and no longer available. If the panel was supplied with 2 & 3-pole FAL breakers, 15-100A, and the mounting hardware still exists on the panel, they can be replaced. If ML-1,2, and 3 pole breakers were used, new FAL breakers cannot be added as there are no new replacement connectors available.


CTA-ID : 15309
Was this helpful?
What can we do to improve the information ?