Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 92445 Double Throw Safety Switch?

Issue:
Product Design features

Product Line:
Double Throw Safety Switches

Environment:
Lug wire size

Cause:
Installation

Resolution:
The lugs on this device will accept (2) #4 AWG - 250 kcmil aluminum or copper conductors per phase. Although the lug will accept 350 kcmil conductors, the wire bending space available in the switch restricts the maximum to 250 kcmil conductors.
NOTE: There are NO alternate lugs
 
Was this helpful?
What can we do to improve the information ?