Technical FAQs

Ask a Question

How can a customer tell what voltage DC coil he has installed in his TeSys contactor?

The standard DC voltage will be imprinted on the front of the contactor, just to the left of terminal 14. If it`s a low consumption DC coil, the front of the contactor will be imprinted with the consumption as well as the DC voltage.

CTA-ID : 2000262
Was this helpful?
What can we do to improve the information ?