Technical FAQs

Ask a Question

Is the external handle for a 2510MBR or 2510MCR NEMA 7 & 9 enclosed manual starter available?

Issue: Need an external handle replacement part number for the 2510 type M NEMA 7 & 9 enclosed manual starters

Product Line: 2510 type M manual starters

Environment: Products sold and used in the United States

Cause: Need an external handle replacement part number for the 2510 type M NEMA 7 & 9 enclosed manual starters

Resolution: The 9998HR3 external toggle handle assembly is available as a repair part.


CTA-ID : 14187
Was this helpful?
What can we do to improve the information ?