Technical FAQs

Ask a Question

Customer has an 8903 type LX mechanically held lighting contactor. How many normally closed (NC) poles can they field convert?

They can convert up to 6 poles to NC on a mechanically held 8903 type LX. If the customer requires more than 6 poles normally closed, it is available from the factory only.


CTA-ID : 2000321
Was this helpful?
What can we do to improve the information ?