Technical FAQs

Ask a Question

Is the UFP222RNM Air Conditioning Disconnect a raintight device?

No, this disconnect is UL Listed as a Type 3R device, which is rainproof, not raintight.


CTA-ID : 2000402
Was this helpful?
What can we do to improve the information ?