Technical FAQs

Ask a Question

What is the UL ampere rating of the Vario switch VCCF5?

It is rated 100A per UL standards and 125A per IEC standards.


CTA-ID : 2000462
Was this helpful?
What can we do to improve the information ?