Technical FAQs

Ask a Question

What is the power rating differences between the 8660 Alphapak and the 8660 SSRVS style starters?

Issue: What is the power rating differences between the 8660 Alphapak and the 8660 SSRVS style starters?
 
Product Line: 8660 AlphaPak starters
 
Environment: All
 
Cause:N/A
 
Resolution:
The currect rating abbreviations were:
Alphapak`s SSRVS`s
MD (16 amps) MG (120 amps)
ME (32 amps) MH (200 amps)
MF (64 amps) MJ (320 amps)
MG (128 amps) MK (500 amps)
MM (750 amps).


They voltage codes were:
Alphapak`s SSRVS`s
23 (208 / 230 volts) 11 (200 volts)
46 (380 / 460 volts) 22 (230 /460 volts)
57 (500 / 575 volts) 33 (500 / 575 volts).  NOTE The 8660 AlphaPak SSRVS are obsolete.  Parts, Service, or Support are no longer available.

 
Was this helpful?
What can we do to improve the information ?