Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DTU321 Double Throw Safety Switch?

Issue:
Product features

Product Line:
DT Safety Switch

Environment:
Product features

Cause:
Clarification

Resolution:
The lugs on this device will accept (1) #12 - 2 AWG aluminum or #14 - 2 copper conductors per phase.

 
Was this helpful?
What can we do to improve the information ?