Technical FAQs

Ask a Question

Can the cover of a QO2100BNF, flush mount circuit breaker enclosure, be changed to adapt the enclosure to a surface mount application?

Product Design Features

Product Line:
QO circuit breaker enclosures



No. Although the cover of the QO2100BNS (surface mount) will physically fit onto the QO2100BNF enclosure, we do not recommend this conversion by merely replacing the cover. Replacement covers do not have nameplates or labels applied to them. If a new QO2100BNS were purchased, its cover would physically be able to be placed onto the QO2100BNF enclosure and it would have the appropriate labeling and nameplate.

CTA-ID : 2001204
Was this helpful?
What can we do to improve the information ?