Technical FAQs

Ask a Question

Can you wire R2 relay on the ATV28 drive to a 115Vac light?

Issue:   Can you wire R2 relay on the ATV28 drive to a 115Vac light?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Yes. The R2 relay contacts are rated for 1.5A 250Vac and 30Vdc.


 
Was this helpful?
What can we do to improve the information ?