Technical FAQs

Ask a Question

Can you get a pressure release valve for a 9013FSG?

Product Line:
Class 9013, pumptrol pressure switch, Type FSG

Resolution:
Form X pressure release valves are not an available option on the 9013FSG adjustable differential switches. Can only be factory ordered on the non adjustable differential 9013FHG switches or the adjustable 9013 Type G.  Field installation is not possible.  The brass fitting with the Schraeder valve is, however, replaceable on any of these that came with form X or X1.


CTA-ID : 2002369
Was this helpful?
What can we do to improve the information ?