Technical FAQs

Ask a Question

Are the 9001K potentiometers AC or DC rated?

Product Line:
30 mm push button operators

Resolution:
They may be used on either AC or DC. Rated for 300 volts and 2 watts.


CTA-ID : 13512
Was this helpful?
What can we do to improve the information ?