Technical FAQs

Ask a Question

Are the Multi 9 circuit breakers, both UL489 and IEC 60947-2 versions, suitable for motor loads?<br />

Yes, in particular, the D curve Multi 9 breakers suitable for application with motor loads. The K curve IEC 60947-2 versions are also suitable.


CTA-ID : 2002170
Was this helpful?
What can we do to improve the information ?