Technical FAQs

Ask a Question

What is the number for the field installed mechanial interlock for two 8502 Type SGO size 5 contactors?

Sizes 5 & 6 mechanical interlocks are available for replacement purposes only for a mechanically interlocked set of contactors/starters previously supplied by Square D. They are not for use in converting a non-reversing contactor or starter to a reversing pair. Following are the available mechanical interlocks for sizes 5 & 6:
Size 5 to Size 5 interlock - 31099-002-50
Size 5 to Size 6 interlock - 31099-002-51
Size 6 to Size 6 interlock - 31099-002-52


CTA-ID : 15568
Was this helpful?
What can we do to improve the information ?