Technical FAQs

Ask a Question

Can the 115/240 vac pilot light provided as standard with the 2510F be used on 277 vac application?

Issue: Can the 115/240 vac pilot light provided as standard with the 2510F be used on 277 vac application?

Product Line: 2510 type F manual starters with pilot light

Environment: Products sold and used in the United States

Cause: Would like to use a 2510 type F manual starter with pilot light on 277VAC

Resolution: Yes, this is a neon type pilot light which will glow a little brighter and electrical life will slightly reduced when applied at 277 vac.


CTA-ID : 14127
Was this helpful?
What can we do to improve the information ?