Technical FAQs

Ask a Question

What is the Terminal Lug data for the H600SN solid neutral assembly?

Issue:
Product features

Product Line:
Heavy Duty Safety Switch

Environment:
Main lug wire size

Cause:
Installation

Resolution:
This neutral has a wire range of (4) #1 AWG - 750 kcmil copper or (4) #2/0 AWG - 750 kcmil aluminum (2 incoming - 2 outgoing conductors). The Service Ground Lug wire range is (1) #4/0 AWG - 300 kcmil aluminum or copper conductor.


CTA-ID : 15496
Was this helpful?
What can we do to improve the information ?