Technical FAQs

Ask a Question

What is H13 suffix on a 9001KS43J1H13 selector switch?

Product Line:
9001 push buttons, 30MM

Resolution:
This H suffix is a contact assembly code. These codes are used to indicate what contact blocks are to be assembled to the operator. H13 indicates a 9001 KA1 is mounted in position 2.


CTA-ID : 2002995
Was this helpful?
What can we do to improve the information ?