Technical FAQs

Ask a Question

What is the part number for replacement cover screws used with QO and Homeline load center covers?

Product Line:
Load Centers

Environment:
QO and HOM load center covers

Resolution:
The 3/4" long replacement cover screw is part #4020513002K, this is a bag of 10 screws. The 1/2" long replacement screw,(typically used for a deadfront piece) is part #4020513001K, this is also a bag of 10 screws. 


CTA-ID : 2003295
Was this helpful?
What can we do to improve the information ?