Technical FAQs

Ask a Question

What kind of noise suppression is available for the DC coils for TeSys D-Line contactors ?

Issue:
Noise suppression needed for LC1D or LC2D contactor with DC control coil

Product Line:
IEC contactors and starters

Environment:
Products sold and used in the United States

Cause:
DC coils can be noisier than AC control coils

Resolution:
The TeSys LC1D09 through LC1D38 with DC control coils are supplied as standard with integral noise suppression, bi-directional diode type.















































CTA-ID : 2002635
Was this helpful?
What can we do to improve the information ?