Technical FAQs

Ask a Question

What is the number of switching operations of Square D, 600A, General Duty, E-Series Safety Switches? These ratings are also sometimes referred to as Endurance operations and Horsepower-overload operations.

Issue:
Product Design Features

Product Line:
General Duty Safety Switches

Environment:
Mechanical Endurance

Cause:
Application

Resolution:
For Safety Switches, the standard for design and testing of the number of switching operations is governed by UL98 and NEMA KS-1.There are two separate tests: (1) Endurance Test, and (2) Horsepower-overload test. The below table shows the minimum number of operations required (OFF to ON to OFF) by UL and NEMA, as well as the number of operations required by Square D.

NUMBER OF OPERATIONS
Square D Safety Switches (E-series)
600A, General Duty
-------------------------Endurance test # of ops------------------. . . . . . . ----HP test # of ops
test stds.....rated Load*...... No-Load...... total (L + NL) . . . . . . . . . . . . . at rated HP**
UL...................1000.............4000...............5000 . . . . . . . . . . . . . . . . . . . . 10
NEMA......... ...1000....... ......4000..............5000 . . . . . . . . . . . . . . . . . . . . 10
Square D.........1000.............4000...............5000 . . . . . . . . . . . . . . . . . . . . 10
* endurance test done at switch rated Load current
** horsepower test - make/break motor inrush/locked rotor current at rated HP



CTA-ID : 2003380
Was this helpful?
What can we do to improve the information ?