Technical FAQs

Ask a Question

What is the acceptable wire sizes for the 8502SF or 8536SF controllers?

Power = 8 awg to 250 mcm, box lug, solid or stranded, copper wire only.

Control = #16 to #12 awg, wire clamp, solid or stranded, copper wire
only.

This also applies to all 8538, 8539, 8606, 8630, 8640, 8702, 8736, 8738, 8739, 8810, 8903, 8940 (except IEC style), and 8941 devices.



CTA-ID : 2004153
Was this helpful?
What can we do to improve the information ?