Technical FAQs

Ask a Question

QO2175SB Pole Spaces

Issue:
How many pole spaces does the QO2175SB use?

Product Line:
QO Surge suppressor products sold and supported in the USA.

Environment
:
Application/installation .

Cause:
When installing the QO2175SB in a panelboard or load center, it is important to realize that this device utilizes two pole spaces in the panel or load center.

Resolution:
The QO2175SB uses 2 pole spaces in the QO load center, NQ or NQOD panelboard




CTA-ID : 2004428
Was this helpful?
What can we do to improve the information ?