Technical FAQs

Ask a Question

Does the Q23225NF include an equipment ground kit?

Issue: Does the Q23225NF include an equipment ground Product Line: Panelboards. Environment: Products sold in the United States. Cause: Product features. Resolution: Yes, a PKOGTA2 is included with this device. This kit consists of two lugs, suitable for #6 - 2/0 aluminum or #10-2/0 copper conductors. CTA-ID : 2003631
Was this helpful?
What can we do to improve the information ?