Technical FAQs

Ask a Question

Does the Q23225NRB include an equipment ground kit?

Issue:
Product Feature

Product Line:
Circuit Breaker Enclosure

Cause:
Product Feature

Resolution:
Yes, a PKOGTA2 is included with this device. This kit consists of two lugs, suitable for #6 - 2/0 aluminum or #10-2/0 copper conductors.


CTA-ID : 2003629
Was this helpful?
What can we do to improve the information ?