Technical FAQs

Ask a Question

Which start stop push button kit is used for a NEMA 1 enclosed combination starter?

Use the 9999 SA2 for NEMA 1 enclosed combination starters, sizes 0 through 3.


CTA-ID : 2004453
Was this helpful?
What can we do to improve the information ?