Original Equipment Manufacturers


                       
                       
                       

                      Success stories - HVAC & R

                       
                       

                      Refrigeration system integrator (Canada)

                         A Canadian refrigeration system integrator sought to improve energy conservation through a decentralised system to independently control temperatures. The installation would have to incorporate an easy programming tool for simplified communication, as well as ease of implementation and maintenance.

                      Benefits
                      - 22% energy saving for the end user
                      - Reduced overall wiring and product cost
                      - Direct communication between the independently controlled cold producer, tank and unit

                      Main customer requirements

                      Operating energy cost reduction
                      - Decentralised automated system architecture
                      - High-performance regulation functions
                         

                      Overall solution cost reduction
                      - Reduced wiring time
                      - Reduced installation errors
                      - Reduced equipment costs

                      Improved communication network performance
                      - Communication of all systems with central supervision for monitoring and configuration functions

                      Our answer
                      An open, flexible solution featuring the Twido Compact controller, Ethernet and the PT100/PT10008-input temperature extension module delivers:
                      - Eight inputs instead of the usual four
                      - Ethernet connectivity for direct communication