Original Equipment Manufacturers


                       
                       
                       

                      Success stories - Material handling

                      Updating an automation solution with a tracking system

                       
                       
                        A French vehicle manufacturer needed to integrate a tracking system into an existing automation system. The company aimed to achieve simple, economical interfacing with the installed programmable logic controller (PLC) network.

                       

                      Benefits
                      - 20% reduction in the overall cost of investment, installation and implementation
                      - Facilitated integration into the existing PLC network
                      - Ease of installation and maintenance through product availability

                      Main customer requirements 
                      - Solution integration without modification of existing PLC programmes
                      - Adaptation of protocol and physical line between PLCs and the identification system
                      - Simplified programming and installation
                      - Improved production reliability
                      - Optimisation of installed equipment maintenance

                         

                      Our answer 
                      The tracking system combines the highly open Twido compact programmable controller and Ositrack RFID system.