Original Equipment Manufacturers


                       
                       
                       

                      Success stories - Simple machines

                       
                       

                      Vehicle manufacturer (Finland)

                        Our customer, a Finnish vehicle manufacturer, operates in extreme climatic, corrosive and mechanical conditions. The firm decided to develop a robust unit capable of being mounted directly on the machine frame.

                       

                      Benefits
                      - Exceptional resistance to severe environments (down to -20°)
                      - Simplified installation due to an enclosure-free mounting
                      - Significantly improved communication performance
                      - User-friendly interface featuring data management and video streaming

                      Main customer requirements
                      - Extreme temperature resistance of devices
                      - Resistance to regular vehicle high-pressure cleaning
                      - Shock and vibration resistance
                      - Touch-screen and joystick interfaces
                      - Reduced installation time

                          

                      Our answer
                      Specially designed for use in severe conditions, our solution comprises the following components:
                      - Twido Extreme programmable controller
                      - Interfacing capabilities (Modbus, CANopen and CANJ1939 integrated in Twido Extreme)
                      - Advantys FTB and Magelis XBT GT