Services


                                                                           
                                                                           
                                                                           

                                                                          Arc Flash Solutions

                                                                           
                                                                           

                                                                          Equipment solutions to reduce arc flash hazards

                                                                          Once the assessment has been completed, you may need to modify or upgrade equipment. In many instances, applying upgrade technologies can reduce PPE levels. If you’re planning a new installation, you’ll want to be advised of new technology solutions available. Schneider Electric offers a wide range of solutions to help you mitigate the arc fault risks present in your installation.

                                                                                    

                                                                          Retrofit solutions

                                                                          Masterpact arc flash circuit breakers provide arc flash protection without fuses, using breakthrough technology exclusive to the industry.

                                                                          • Retrofit existing low voltage power circuit breakers using the new arc flash Masterpact NW or NT retrofit and/or direct replacement products. Schneider Canada Services offers direct replacement breakers for many manufacturer’s low and medium voltage breakers, including Allis Chalmers, Federal Pacific, Federal Pioneer, General Electric, ITE/ABB and Westinghouse.


                                                                                  The Comet® H.VIR infrared viewing window uses a crystalline material that is up to 96% transparent to infrared wavelengths. This ensures accurate infrared scanning while maintaining the equipment’s NEMA or IP ingress rating.
                                                                          • Install H.VIR Comet Infrared (IR) viewing windows, which allow diagnostic IR scanning without removing equipment covers to improve worker safety while assessing equipment condition. The crystal material used in the H.VIR windows is up to 96% transparent to infrared wavelengths, which ensures accurate IR scanning while maintaining the equipment’s NEMA or IEC/EN IP ingress rating.


                                                                                  The Square D Arc Terminator system detects and controls the effects of arcing faults, extinguishing arcs in less than 1/4 of a cycle.
                                                                          • Install the Square D arc terminator device retrofitted into existing MasterClad® medium voltage switchgear to reduce or eliminate arc flash hazards.
                                                                          • Install auto rack remote racking system for the existing medium voltage circuit breakers to help keep workers at a safe distance from potential arc flash locations.


                                                                                          Sepam medium voltage and Carriere low voltage protective relays provide LSIG functionality to reduce tripping times under arc flash conditions.
                                                                          • Upgrade low or medium voltage breakers with Sepam medium voltage protection relays or Carriere low voltage protective relays. Both offer LSIG functionality to help reduce breaker tripping times. Sepam protective relays allow you to switch between two protective relay settings. This allows you to select the more sensitive settings based upon arc fault conditions when working on equipment.

                                                                          New equipment solutions

                                                                          When designing a new system, contact your Schneider Electric consulting engineering specialist to help with the specification of our new Square D Powerzone 4 low voltage switchgear, which can include Masterpact NW or NT arc flash branch circuit breakers.
                                                                          As an alternative to arc resistant switchgear, a Square D arc terminator device can be installed in one cell of a Square D MasterClad® medium voltage switchgear lineup, protecting up to 10 breakers. The Arc Terminator system detects and controls the effects of arcing faults. It extinguishes arcs in less than 1/4 of a cycle, significantly minimizing equipment damage and reducing equipment downtime.

                                                                            
                                                                           
                                                                          To know more

                                                                          To know more 

                                                                          Requests for Solutions, Products and Services information

                                                                          • 24 Hour Service

                                                                          Call 1 (800) 265-3374