When problems arise due to the increasing need for maintenance and the scarcity of spare parts for aging Merlin Gerin Type DA or Selpact circuit breakers,
Schneider Canada Services offers a new solution : Replace the older device with modern Masterpact circuit breakers. Masterpact power circuit breakers are IEC/UL/ ANSI/ NEMA listed devices with all the advantages supplied by the latest technology :
Advantages
- Reduced Downtime - using prefabricated mounting and connection kits
- Cost-efficient Solution
- Reduced Maintenance Requirements
- Improved Reliability
- Improved Safety
- Extended use of the installed Switchgear