Maintain the value and use of existing electrical equipment with genuine replacement parts
- Federal Pioneer
- Merlin Gerin
- Modicon
- Square D
- Telemecanique
|
|
The Services Solution Centre exists to enhance the service level provided by these brands. A computerized inventory system provides instant confirmation of availability and convenient access to these high-quality parts through satellite operations from coast-to-coast. However, this unit of Schneider Canada Services is much more than a warehouse. Parts for any make of equipment, of any vintage, are available through the use of a quality-controlled reverse engineering process. Many repair and refurbishment devices and programmes can also be provided.
Repair Services:
Products are available to repair, extend or enlarge adequately performing older installations. For example, The Services Solution Centre can provide:
- Federal Pioneer H3 Air Circuit Breakers
- Units for Square D, Models 2, 3 or 4 Motor Control Centres
- Lengths, fittings and take-off devices for Federal Pioneer bus duct and Square D busway
- Repair or replacement of non-current Square D and Telemecanique solid-state drives and soft-starts
The continuous development programmes of the Brands of Schneider Electric result in products and technologies that make electrical systems more reliable, efficient and safer. The Services Solution Centre has designed ways to add these improvements to existing installations, including:
- Conversion of low voltage air circuit breakers to solid-state trip units
- Square D, Model 4 Motor Control Centre refurbishment
- Federal Pioneer Medium Voltage Motor Starters upgraded with vacuum contactors
- Medium Voltage Circuit Breaker replacements